Hi,
Can someone tell me what is the best way to route analog lines on a PCB, that are carrying the current from a photodiode to an A/D current integrator such as the DDC114?
The currents are pretty low, on the order of pA or even less, along about 0.5sec.
I've seen people saying it is best to place them in an inner layer, between two grounded layer, in order to shield them, but then it might create some parasitic capacitance...
On the other hand, I've been told that introducing via holes along this kind of low current lines can introduce offset voltages arising over the via holes.
Any comments on this subject?
Thanks,
Boaz