Hi,
We are planing to use the TMP007 for our application where we need to measure objects on a conveyor belt where different objects with different temperatures +/- 20C are moving past the sensor at close proximity.
When the belt is idle the sensor outputs ~22C but when a object stops in front of the sensor it takes 5-6 seconds before the temperature settles at ~37C, why?
The objects are big so the objects are 100% in FOV.
We have tried with both our custom design and the EVM with the same results, the sensor is configured for 4Hz output, TC enabled, alert asserted on temp ready. We could also reproduce the same behavior with just putting our hand over the EVM
Please advice!