hello I have a question I don't want to use the OS feature in the chip, should I leave it floating or tide it to ground?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello I have a question I don't want to use the OS feature in the chip, should I leave it floating or tide it to ground?
thanks
Hello Sonny,
I moved this to the Temp Sensors Forum; the O.S. pin is open-collector and technically can be left open. However, good design practices would suggest connecting a pull-up resistor, if for nothing else, just to have a monitor function during debug. As stated in the datasheet:
7.5.6 O.S. Output
The O.S. output is an open-drain output and does not have an internal pullup. A “high” level will not be observed on this pin until pullup current is provided from some external source, typically a pullup resistor. Choice of resistor value depends on many system factors but, in general, the pullup resistor should be as large as possible. This will minimize any errors due to internal heating of the LM75A. The maximum resistance of the pullup, based on LM75A specification for High Level Output Current, to provide a 2-V high level, is 30 kΩ.
~Leonard