Hi Team,
We have a customer looking to use AMC6821 in their design to control the fan and has a couple of questions. They are trying to use this chip in as much of a standalone application as possible. They are using a 16-bit MCU with an I2C interface to the AMC6821 to load the various register settings (they have checked the various electrical specs and it looks like it should work). They will try to run the chip in “Auto Temperature Fan Mode” with [FDRC1:FDRC0] = [11] for the “maximum fast-speed calculated control mode.”
In this mode, is it required that they add a remote temperature sensor or could they leave the IN+ and IN- pins N/C?
PWM-Out: can this be attached directly to the PWM input on most 4 wire fans (with a pull-up resistor to account for the open-drain)? They hope to use this fan.
Thanks for the assistance,
SSF