Other Parts Discussed in Thread: TMP103, LMT70, LMT01
Hi,
How much the thermal response time of TMP468 at local temperature at still air?
What is the local temperature sensor with the fastest response time at TI?
Regards,
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ACGUY,
I need to double check with the team on the LMT70 time constant (it seems quite long for that package).
Still air time constant:
LMT01 (DFN) ~10 sec
LMT8x family (SC70) ~10 sec
I don't have still air data for TMP103 but I'm confident that it's much faster than LMT01 or LMT8x since it is much smaller package However,
it will depend if you're trying to measure board or ambient temperature. If you're measuring board then TMP103 would be a good choice and since it's digital zero calibration is required for guaranteed accuracy. If you're measuring air, you will need to thermally isolate the device from the board using pcb cut-outs.
The pcb may contribute to the thermal mass and slow the response of the device so layout is critical.
Summary:
For ambient measurement I would recommend the thru-hole LMT01 (LPG). This has a 20s thermal time constant.
For board measurement I would recommend TMP103 (DSBGA). I confident that it's one of the fastest SMD devices we have.
If you can, go with digital and you don't have to calibrate for guaranteed specs. If you have to use analog instead, I would recommend LMT70 for SMD.
-Kelvin