We're not sure why our device is reading the temperature value off by 0.5 C to 1.0 C. We are comparing it to other accurate and calibrated devices placed in the same conditions.
We get the same error if we connect it to the sensor on our board OR the sensor part of the LMT70EVM (We hard wired it to the sensor).
Our temperature range is from -30 C to +70 C
We are interfacing it to the Nordic nRF52832
This is an urgent request as we just finalized the firmware and are trying to resolve this issue. We have purchased several thousands of these sensors and are ready for production. Not sure why we're getting this issue now.
Is there anything we can do in the calculations?
If it's easier and faster I can contact customer support.
Thanks very much.
Arif