we are working an a vacuum food processor. Our request is to measure the temperature of the food when it is in the plastc bag, after processing. Plastic bag can be polyammide or polypropylene. Is this kind of plastic suitable for Ir reading?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
we are working an a vacuum food processor. Our request is to measure the temperature of the food when it is in the plastc bag, after processing. Plastic bag can be polyammide or polypropylene. Is this kind of plastic suitable for Ir reading?
I don't know about the polyamide. But I worked with polypropylene. The samples which we used are not visual transpared and looked milky white. We used 0.4mm film. It is not very flexible and lower the IR signal strength by 50%.