I’m running into an interesting issue on the TMP108, was wondering if anyone can help or have seen this before...
On our board, I see that the ALERT (C1) pin of TMP108 keeps toggling @ 1Hz. I cannot turn this off. I have set all the registers of the TMP accordingly:
- Here are my register settings:
- CONFIG: (interrupt mode)
i. BYTE1: 0x06
ii. BYTE2: 0x30
- High temp threshold (50 degrees C)
i. BYTE1: 0x03
ii. BYTE2: 0x20
- LOW temp threshold (0 degrees C)
i. BYTE1: 0x00
ii. BYTE2: 0x00
- I am reading the CFG register, and the register is reading 0x06, 0x30 (no FL or FH)
- Current room temperature reads 24 degrees C
- We are using this part at 1.8V.
So I don’t understand why the ALERT pin is toggling, or how I can get it to stop....