Hello guys,
One of our customers is evaluationg TMP112 on their own board. They have faced a trouble. The trouble and question are the followings.
One TMP112 and a MCU are mounted on their board. Also a actuator which drives high current is mounted on it. The MCU can read temperature data from TMP112 without any problem befor the actuator on/off. But after the actuator on/off, the temperature data can't be read by the MCU with I2C communication problem. Then TMP112 doesn't send any temperature data through I2C (SDA,SCL) even if MCU sends read command with intervals more than 100ms. After the board power is off and on, the I2C communication returns to the normal I2C communication and the temperature data can be read correctly. The customer question is that is ther any way to restart or reset I2C communication of TMP112 without the device power off and on?
Could you please give me your reply or comment? These would be much appreciated.
Best regards,
Kazuya Nakai.