Hello Sirs,
We need to use two LM96000 at same SMBUS system for six PWM and six TACH meter.
So need to pull correct level for PWM3/ADD_enable and TACH4/ADD_sel .
Do you have comment for :
LM96000#1 pull up 10K to 3.3V for PWM1~3 . Slave address is default "0x2e"
LM96000#2 pull up 10K to 3.3V for PWM1~2 . How to treat PWM3/ADD_enable for this is open-drain pin ? How to treat TACH4/ADD_sel ? What's slave address for this device ?
Many thanks !
I hear this description. Does it mean I can't use TACH4 and PWM3 for 2nd LM96000 ??
When using the non-default addresses the TACH4
and PWM3 will not function. As shown in the timing diagram the Address Enable pin must remain low in order for
the latched address to remain in effect. If the address enable pin is pulled high after the first SMBus
communication, then the LM96000 SMBus address will revert to the default value (2Eh) after the first five clocks
of next SMBus communication