Hi all,
I am using AWR1642 with DCA1000EVM to record radar data , with the same configuration used in the vital signs lab.
In the vital signs config, the chirp period is 50 micro seconds and the frame period is 50 ms and in my case (also vital signs case) they are using only one chirp per frame (two chirps but one for processing), so why should the frame period is much more higher than the chirp period, is it useless to have a frame with 50 ms which is >>> 50 micro second ? should the frame period be just a bit high than the chirp config ? because otherwise the almost the hole frame will be empty is it just contain one chirp with 50 micro sec (1/1000 * frame period ) ! or am I understanding it the wrong way ?
I sow the details in the vital signs lab document and didn't found an explanation to this .
my frame config: ar1.FrameConfig(0, 0, 6000 , 1, 50 , 0 , 1)
my profile config : ar1.ProfileConfig(0, 77, 7.01, 6, 57, 0, 0, 0, 0, 0, 0, 70.106, 1, 100, 2000, 0, 0, 40)
thank you in advance,
Ahmed