Other Parts Discussed in Thread: IWR1443
Tool/software: Linux
Hi,
The IWR1443BOOST config files with the Demo Visualizer have a max range resolution of 4cm. Is it possible to get better range resolution?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi,
The IWR1443BOOST config files with the Demo Visualizer have a max range resolution of 4cm. Is it possible to get better range resolution?
Thank you.
Hi Rupak,
Range Resolution is a function of the RF bandwidth of the chirp and it is defined as R-res = c/2B where c is the speed of light and B is the effective chirp bandwidth.
The IWR1443 has a maximum continuous chirp bandwidth of 4GHz (77GHz to 81GHz) which corresponds to a best case range resolution of ~4cm following the above equation. This is what the "Best Range Resolution" option configures in the OOB Demo.
Please note that while the best case range resolution is ~4cm, you can achieve sub-millimeter range accuracy with the device as discussed in the following thread:
IWR1443BOOST: Sub-millimeter accuracy distance measurement on a short range (from 5 to 30cm)
Please mark this thread answered if your query was recolved otherwise get back if you have more questions on this topic.
Thanks
-Nitin