This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

AWR1642: DCA1000+AWR1642,spi connect

Intellectual 385 points

Replies: 18

Views: 1135

Part Number: AWR1642

I followed the steps in ppt (mmWave Sensor Raw Data Capture Using the DCA1000 Board and mmWave Studio). When I proceeded to the 'Click the SPI Connect button' step, I did not see 'SPI Disconnect', then I tried erase Flash on xWR14xx/xWR16xx EVM, I followed the steps to re-operate, but the result still does not appear 'SPI Disconnect', what is the reason?This is a screenshot of my current operation, and ouput.

GM: Constructor
GM: Wed Jan 09 10:05:06 2019
RSTD.Transmit("/Settings")
[10:05:06]
[10:05:06] ### Running Startup script: "C:\ti\mmwave_studio_02_00_00_02\mmWaveStudio\Scripts\Startup.lua" ###
[10:05:07] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[10:05:07] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[10:05:07] Scripter ignored: Attempt to UnBuild() again or before Build.
[10:05:07] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_00_00_02\\mmWaveStudio\\Clients\\\\LabClient.dll")
[10:05:07] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[10:05:07] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[10:05:07] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[10:05:07] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[10:05:07] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[10:05:07] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_00_00_02\\mmWaveStudio\\RunTime\\SAL.dll")
[10:05:07] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[10:05:07] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[10:05:07] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[10:05:07] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[10:05:07] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[10:05:07] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[10:05:07] RSTD.Transmit("/")
[10:05:07] RSTD.SaveSettings(): Settings saved to "C:\Users\Administrator\AppData\Roaming\RSTD\config.xml"
[10:05:07] RSTD.Build()
[10:05:07] RSTD.SaveSettings(): Settings saved to "C:\Users\Administrator\AppData\Roaming\RSTD\config.xml"
[10:05:07] RSTD.Transmit("/")
[10:05:07] RSTD.AL_Build()
[10:05:07] RSTD.AL_LoadXml()
[10:05:07] RSTD.Transmit("/")
[10:05:07] RSTD.AL_Init()
[10:05:07] RSTD.Clients_Build()
[10:05:07] GM: Init
[10:05:07] GM: Loaded 'C:\ti\mmwave_studio_02_00_00_02\mmWaveStudio\Clients\\LabClient.dll'
[10:05:07] GM: 1 Guest (s) init
[10:05:07] GM: 1 Module(s) init
[10:05:07] GM: 2 Tab (s) init
[10:05:07] RSTD.Client_LoadXml()
[10:05:07] [RadarAPI]: Starting Matlab Engine..
[10:05:11] [RadarAPI]: Matlab Engine Started!
[10:05:14] [RadarAPI]: ar1.LoadSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
[10:05:14] TESTING = false
[10:05:14]
[10:05:14] ***Script completed successfully.***
[10:05:18] [RadarAPI]: Opening Gpio Control Port()
[10:05:18] [RadarAPI]: Status: Passed
[10:05:19] [RadarAPI]: Opening Board Control Port()
[10:05:19] [RadarAPI]: Status: Passed
[10:05:20] [RadarAPI]: ar1.FullReset()
[10:05:20] [RadarAPI]: Status: Passed
[10:05:20] [RadarAPI]: Closing Board Control Port()
[10:05:20] [RadarAPI]: Status: Passed
[10:05:21] [RadarAPI]: Closing Gpio Control Port()
[10:05:21] [RadarAPI]: Status: Passed
[10:05:21] [RadarAPI]: ar1.SOPControl(2)
[10:05:21] [RadarAPI]: Status: Passed
[10:05:22] [RadarAPI]: ar1.Connect(4,115200,1000)
[10:05:23] [RadarAPI]: ar1.Calling_IsConnected()
[10:05:25] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[10:05:25] [RadarAPI]: Status: Passed
[10:05:25] [RadarAPI]: RS232 is not connected ..!!!!
[10:05:25] [RadarAPI]: ar1.frequencyBandSelection("77G")
[10:05:25] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[10:05:25] [RadarAPI]: Status: Passed
[10:05:25] Device Status : XWR1642/ASIL-B/SOP:2/ES:2
[10:05:26] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[10:05:26] [RadarAPI]: Status: Passed
[10:05:26] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[10:05:26] [RadarAPI]: Status: Passed
[10:05:26] Device Status : XWR1642/ASIL-B/SOP:2/ES:2
[10:05:26] [RadarAPI]: ar1.SaveSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
[10:05:34] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_00_00_02\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr16xx_radarss.bin")
[10:05:35] [RadarAPI]: Downloading BSS Patch RPRC Binary..
[10:05:42] [RadarAPI]: ar1.GetBSSFwVersion()
[10:05:42] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[10:05:43] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[10:05:43] [RadarAPI]: BSSPatchFwVersion:(01.02.00.03 (24/10/18))
[10:05:45] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_00_00_02\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr16xx_masterss.bin")
[10:05:45] [RadarAPI]: Downloading MSS RPRC Binary..

  • Hi, I have the same problem, waiting for reply. TSW1400EVM+AWR1642BOOOST

  • In reply to gao song:

    Hi Wei,

    Can you please confirm if you have set the SOP mode jumpers correctly on the EVM?

    Thanks,
    Anand
  • In reply to gao song:

    Hi Gao,

    The TSW1400+AWR1642 is a different combination. Could you please raise a separate thread to discuss it?

    Please provide more detailed information and if possible screenshots. Please also confirm that you are using a 5V 3A or better power supply with the TSW1400 as it is draws a lot of current when the FPGA boots up.

    Best Regards,
    Anand
  • In reply to Anand Gadiyar:

    I confirm i mount jumpers on the sop0 and sop1 pins.

  • In reply to Anand Gadiyar:

    i use a 5V 2A power supply for DCA1000 and 5V 3A power supply for AWR1642.
  • In reply to Anand Gadiyar:

    Hi Anand

    I will raise a separate thread to discuss it.

    i use a 5V 2.1A power supply for TSW1400EVM and 5V 2.1A power supply for AWR1642BOOST.


    Best Regards,

    Gao

  • In reply to Anand Gadiyar:

    Hi Anand and Wei,

    I turned S2 to SPI direction in AWR1642BOOST and JP1&JP2&JP3&JP4 to FTDI direction in MMWAVE-DEVPACK. Finnally i solved the problem.

    Best Regards,
    Gao

  • In reply to wei liu62:

    Hi Wei,

    Can you please confirm if the demo application included with the SDK 2.0 or later is working with the mmwave demo visualizer on this board?

    Thanks,
    Anand
  • In reply to Anand Gadiyar:

    Yes,i can confirm.Before purchasing DCA1000, I have used AWR1642 working with the mmwave demo visualizer.

  • In reply to Anand Gadiyar:

    this is my hardware.(At this point, the display of mmWaveStudio is the first image above.)

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.