Hi,
I would like to understand how EDMA works.
I look at Figure 12-6 pp.1179 of Technical Reference Manual SWRU522C.
I look at code from lab0015_pplcount_68xx dss_data_path.c line 443
EDMAutil_configType1 configured EDMA with following parameters
aCount = 512
bCount = 2
cCount = 1
sourceBindex = 1024
destinationBindex = 0
sourceCindex = 0
destinationCindex = 0
The EDMA is programmed as an "A-Synchronized transfer"
There are two transfers of 512 bytes because bCount is 2.
Is second transfer of 512 bytes have same destination addres as first one because destinationBindex is zero?
Regards,
Gennadii