Other Parts Discussed in Thread: LM20, LMT70, LM70
Hi Team,
Please recommend a device which can output < 1000mV at 100℃. TMP235‘s output is a bit high at 100℃。 thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Yue -
I think proposing they use a voltage divider with a part like the LMT70 would be the cleanest way with our devices, given this narrow band of operation. the device swings from 1375mV @ -55C to 302mV @ 150C. if they use two equally valued resistors, for example, the range out to the ADC would swing from 0.687 to 0.15V, within the range of their requirement.