Other Parts Discussed in Thread: FDC2114,
Error Channel
Indicates which channel has generated a Flag or Error. Once
flagged, any reported error is latched and maintained until either
the STATUS register or the DATA_CHx register corresponding
to the Error Channel is read.
b00: Channel 0 is source of flag or error.
b01: Channel 1 is source of flag or error.
b10: Channel 2 is source of flag or error (FDC2114, FDC2214
only).
b11: Channel 3 is source of flag or error (FDC2114, FDC2214
only)
question:
the STATUS reg val is 0x404C, and what's the meaning of Error Channel ?
how i can distinguish this val whether a Flag or Error ?
what's the reason to cause this ERR_CHAN field set 1 ?
how to remove the error flag ?
If anyone has any advice I would be most appreciative.
Best regards !
ps,
0X19 REG_STATUS_CONFIG val is 0x3821.