This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC4067: CD74HC4067

Part Number: CD74HC4067

hello TI,

 the CD74HC4067  E=1 ,select no chanel ,the commen input or output connect to gnd,and the i0~i15 connect to dc:300v, this connect is ok?

  • User4931861,

    Placing 300V on the CD74HC4067 is greater than the abs max voltage stated in this datasheet and will damage the device.

    Would you be able to describe more detail about the application you are trying to achieve. maybe with a diagram?

    Thank you,
    Adam