Hi,
Need to select a SPDT multiplexer which would select one of the inputs and connect to the output based on the select inputs of the multiplexer
Input 1 : A sense signal ( Output of a TLV271 opamp)
Input 2 : A sense signal ( Output of a TLV271 opamp)
Based on the select signal (0 or 1) I need one of the inputs to be relayed to the output pin of the multiplexer.
Requirements:
Bandwidth > 10MHz ( To make sure that the relayed signal does not have any phase lag introduced).
Resistance of the path < 10E
Current carrying capability of the switch : < 10mA (Ok, even if its more)
Supply voltage: 5V and 12V( Two different cases)
Regards,
Rajesh Sura