This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

MUX36S08: Schematic review about the application of MUX36S08

Prodigy 210 points

Replies: 1

Views: 76

Part Number: MUX36S08

Hi Team,

Customer wants to use MUX36S08 to change the gain of amplifier, please take your time to review the schematic and give some suggestions to possible issues. This is a great chance for our MUX36S08 and OPA2196.

Below is the detailed schematic, the exact number of amplifier is OPA2196.

Best Regards,

Stanley Dai.

  • Hi Stanley,

    The MUX36S08  is a good option to select the gain of amplifier. it offers Low RON  (125 Ohm) for better linearity and lower distortion, Low leakage current (1pA) for precision along with Low ON capacitance (9.4pF) and low charge injection (0.3pC). it works with dual supplies (±5 V to ±18 V) or a single supply (10 V to 36 V).

    Looking at the schematic, I don't see any potential issues.

    Please let me know if you have further questions.

    Thanks

    Saminah

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.