Is there a typical Iq spec for the SN74LV4052APWR?
The datasheet only specs 20uA max at 5V.
Is there a reduction of typical Iq at 3.3V operation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a typical Iq spec for the SN74LV4052APWR?
The datasheet only specs 20uA max at 5V.
Is there a reduction of typical Iq at 3.3V operation?
Hello,
I went into the lab and did a quick Iq measurement following the way the data sheet specs it:
Where int INH pin or VI is tied to GND and ramped up the temperature to 85C since Iq rises with temperature.
The measured current for 3.3V:
The measured current for 5V:
Please understand that these are typical values that I saw on a few devices, so the max value one will ever see is what we spec in the datasheet.
Thank you,
Louie