Tool/software: Code Composer Studio
Hello,
This is my first post in this forum. I am new to this field and not a expert in this area.
I'm trying to manually program CC2640 without PCB board. I manually soldered the pins and successfully connected the wires to JTAG pins.
When I run CCS and load my program, it uploads successfully. However, the device doesn't pop up on Flash Programmer 2. (Sometimes it does, and sometimes it doesn't).
When Flash Programmer 2 picks up CC2640 chip and when I click right button on mouse and press connect, it fails.
What I'm curious is... using CCS it seems to upload the program without any errors. But I am not sure if that means my program is successfully uploaded.
Based on my description, does it seem like the program is uploaded? I am asking because Flash Programmer 2 doesn't seem to detect CC2640 reliably...