Tool/software: TI C/C++ Compiler
I need to make some change to an old project that use MSP430 TI 4.4.5 compiler and there is a warning message.
warning #10204-D: could not resolve index library "libmath.a" to a compatible
Then, I change the build output format to ELF to resolve this warning message. Once I do that, I realize the linker no longer place the following variable to the specific memory location anymore. It works if I change the output back to legacy COFF. Do I miss anything?
#pragma DATA_SECTION(Image_boot, ".memlocation")
const unsigned char Image_boot[1024]={
#include "boot_sym.dat"
};
Thanks,
Jonathan