Other Parts Discussed in Thread: TIDA-01606
Tool/software: Code Composer Studio
I have selected this controller TMS320F28034 also think that this software applies to our case sprabt4a-!
and or this too tidcfh3 and this hardware TIDA-01606_Power CardE4_Sch. We have already designed our hardware
based on this TIDA-01606_Power CardE4_Sch.
We monitor 24 situations which is scanning external multiplexer chip of scaled down voltage exceeds +/- 25%. at 2,5 Volts and additional
temperature monitoring using LMT87LPM and three current monitoring of three phase using AMC1306 and three phase grid voltage and inverter three phase
voltage monitor. This is all about it.
I need modify the above to suit my need and fit my selection of TMS320F28034
I look forward to hearing from you gays
Thank you and Regards
Dan-Harry
Dawari.Danharry@gmail.com
401 263 5563