Hi,
I have your THS4522 PSPICE model (ths4522.lib, Date: 10/03/2016) and am trying to simulate it in PSPICE. I also tried LTSpice. I have found what I believe to be a problem. PSPICE fails with the error "INTERNAL ERROR -- Overflow, Convert". LTSpice is a little more helpful:
Fatal Error: Unknown parameter "#IND"
in line:
"b:u2:i0:i32:i5:§eitailmin u2:i0:i32:i5:itailmin 0«::::0» v= -1.#IND *v(u2:i0:vcc_int,u2:i0:vee_int)+ -1.#IND "
I've traced it to subckt GmTail (line 602) which is included as a component starting at line 118:
Line
118 XI5 NET026 NET8 0 NET080 VEE VCC NET043 GmItail PARAMS: Choice=1 Gm=1.98838E-01
119 + ITAILMAX_X1=3 ITAILMAX_Y1=76e-3 ITAILMAX_X2=5 ITAILMAX_Y2=76e-3 ITAILMIN_X2=5
120 + ITAILMIN_Y2=77e-3 ITAILMIN_X1=5 ITAILMIN_Y1=77e-3
Subckt GmTail includes the calculation:
644 .PARAM ITAILMIN_SLOPE =
645 + { ( ITAILMIN_Y2 - ITAILMIN_Y1 ) / ( ITAILMIN_X2 - ITAILMIN_X1 ) }
which of course results in division by 0 since ITAILMIN_X2 = ITAILMIN_X1 = 5.
1) Could you fix this error so it simulates?
2) What simulator are you testing with that allows division by 0?
3) It would be nice to have the option of have a simple model for simulating the AC and transient response (quick simulation, low probability of convergence problems).
Thanks
Eric