Other Parts Discussed in Thread: ISO1212,
What are the benefits of using ISO1212 (Isolated 24-V to 60-V Digital Input Receiver) in the implementation of safe torque off functionality in Variable Speed Drives?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the benefits of using ISO1212 (Isolated 24-V to 60-V Digital Input Receiver) in the implementation of safe torque off functionality in Variable Speed Drives?
TIDA-01599 is a TI Reference Design that implements safe torque off functionality in variable speed drives (per IEC61800-5-2).
ISO1212, which is an Isolated 24-V to 60-V Digital Input Receiver, offers the following benefits to implement safe torque off
For additional information about this topic, please refer to section 2.6 "System Design Theory" of the User Guide for TIDA-01599.
You can also download the design files (BOM, Schematic, Gerber) for this reference design from the TIDA-01599 folder.