Other Parts Discussed in Thread: TIDA-00364, UCC27714, UCC27712, UCC27712-Q1
Dear TI Experts:
I found TIDA-01418 is a nice design example.
I hope to apply it in my targeted application: Vbus=86V (max. Vbus=100V ) and rated 3kW (peak 7KW) with 3-Shunt FOC control for a 3-Phase PMSM.
Q: Change the IGBT to NMOSFET
I have found the NMOSFET with Vds=150V, Rds=4.8 mOhm, and Id=171A. Could I directly replace the IGBT: IXYP15N65C3D1 module in the inverter with the NMOSFET I found?
Look forward to hearing from you soon.
Best Regards,
Tang Han