Part Number: TIDA-01501
Hello,
Some signals are not clear how they are connected.
-On the LLC stage schematic, it is unclear how V+ and V- of the LM258AD are connected. The components are named U2 and U10.
-What is U15?
-Is the Signal VTEMP in the LLC stage something else other V_temp on the daughter board?
- is SGND1 in the daughter board not connected to SGND on the LLC stage? I think so so that no short circuit happens on the synchronous rectifier mosfets, Right?
- to which supply is VS_AUX2 in the daughter board connected. The U15 daughter board connector in the LLC Stage Shows that pin2 should be V_temp (not VTEMP) and pin3 should be named VS_AUX2. Unless I misunderstood something.
Thanks very much.
Kind Regards,
Amr