This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP21160: Output Voltage

Part Number: PMP21160

Hi,

The report assumes an output voltage of 24V +/- 5%.

Is there any easy way to modify the design to adjust voltage up to 28V even with lower performance?

thanks