Tool/software: Code Composer Studio
Hi I have the problem, that when Iam connection the sensortag via Bluetooth to an Iphone 5s, the sensortag disconnects immediately and the red light blinks with the following message: The connection has timed out unexpectedly, error 6). I checked the battery status because I thought that battery is to low, but I have still 64 %. I was able to connect all the time without any problems, but now I am encountering this problem.
What could be the cause of this problem?