This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] BLE Qualification : Known Issues and Fixes

Guru 57705 points

Replies: 1

Views: 1450

Part Number: CC2640R2F, CC2642

Please see this thread for Bluetooth Qualification updates.

Customers attempting to create an End-Product listing with our qualified UUIDs, may end up with inconsistencies due to TCRL 2018-1 (Erratum E10734).

For CC2640R2, attached here are test evidence needed to complete the listing; 

These test evidences are based on Category B  which means that they were collected by in house testing (Not PTS). Sniffer and logs must be shared with the end-product listing. Here is an example how;

For Peripheral:

Test Evidence Information

Test Case Verdict (Pass, Fail,  Waived, Referenced)

Test Execution (Date)

Test Equipment Platform

Test Report Reference

IUT Configuration

Integrated QDID

Evidence Notes

Pass

28/03/2019

CC2640R2F

BLE5-1.1.3

D041506

 

For Peripheral+Central:

Test Evidence Information

Test Case Verdict (Pass, Fail,  Waived, Referenced)

Test Execution (Date)

Test Equipment Platform

Test Report Reference

IUT Configuration

Integrated QDID

Evidence Notes

Pass

28/03/2019

CC2640R2F

BLE5-1.1.3

D041507

For CC2642, attached here are test evidence needed to complete the BT5.0 listing; 

     If you are new to the topic and want to learn more on how to qualify your Bluetooth low energy product, please refer to this app note.

     

    Regards, Joakim

     

    • Guru 57705 points
      For any questions on this topic, please hit "ask a related question"

      Regards, Joakim

       

    This thread has been locked.

    If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.