Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
hello ,
1. i'm tring to write two times to uart , some reasne it anly write once per loop !!
1.1 we using Version: 9.1.0.00010 all latest vertion
here is the code :
void *mainThread(void *arg0)
{
uint32_t curtime;
RF_Params rfParams;
UART_init();
ADC_init();
RF_Params_init(&rfParams);
.....
sprintf(str,"Send3 %d bytes O.k {%s} [%s] %d ADC0 %d\r\n",packetLength,&txPacket[2],&rxPacket[2],PacketCompare(&txPacket[2],&rxPacket[2],15), adcValue);
UART_write(uart,str,strlen(str)); // write to urt is o.k
sprintf(str,"execute done %d\r\n",);
UART_write(uart,str,strlen(str)); // does not write to uart ??
please advice