Other Parts Discussed in Thread: CC3200, UNIFLASH
Tool/software: Code Composer Studio
We are developing a WiFi connected sensor board using the the CC3200-LanchXL and are having trouble connecting to are companies Enterprise network. The board connects fine to our secondary network that does not require a user id, only a SSID and passkey. We've tried all the combination for EapMethod and security Types without success. The one thing we noticed is if a break point is placed at the sl_WlanConnect step the variables, only the first 10 characters appear, where the full UID is "usr.new.PerfUser", 16 characters in length. An image of the code block is bellow the variable image. Any insights are welcome.
Thanks, KS