Other Parts Discussed in Thread: Z-STACK
We are working on a temperature and humidity sensor on cc2530. The device has 2 sensors. One temperature and second temperature and humidity. The device reports humidity and temperature at endpoint 1 and the second temperature at endpoint 2. Reaport max time is set to 20 minutes. Reaport value change in temperature is set to 0.2C and humidity to 1%. There are situations when e.g. the temperature on the sensor is not reported for an hour. This occurs when, for example, the humidity often changes during this period. As if max reaport time did not function then.
It also often happens that the report comes not every 20 minutes but e.g. 19 minutes and 58 seconds.