Greetings,
Here is the hardware\setup we are using:
1. Panasonic EVAL_PAN1323ETU evaluation board that has a TI CC256x chip
2. Freescale SoloX Evaluation board with a Cortex A9 processor (i.MX 6)
3. Yocto Linux with BlueZ 5.28 stack
4. TIInit_6.7.16.bts ( found here: https://e2e.ti.com/support/wireless_connectivity/bluetooth_cc256x/f/660/t/441580
We use the hciattach utility that comes with BlueZ to load the combined initialization script and add-on script.
So far we are not able to set up a serial port profile (SPP)...i.e. it does not show up as a serial port (COM port) on a PC.
Ubuntu Linux on the other hand can talk to the module via a rfcomm socket (or port).
Our questions:
1. Will this setup work for a PC? Will it show as a SPP port?
2. If yes, what are the right combination in terms of versions: BlueZ, TI's scripts, and chip version?
Any help on this matter would be greatly appreciated!