Hi,
All these days i was using v1.4R2 with older CC6 compiler where in i had modified A3DP_SNK stack which worked perfectly fine on the hardware. Recently due to my laptop upgrade, i moved to ccs 6.1.3 compiler and with some hickups and from experts help form TI forum i was able to compile v1.4R2 with latest compiler as it failed to compile. Now when i flash the FW, i don't see my BT device evening getting discovered in the scanning. Is there something i need to do in v1.4R2 to work with latest compiler. Please help me out as i am stuck on this from past 1 week and one option i think of is to port the whole code to v1.5R2 which i am bit skeptical without understanding the issue as to why it is not working with v1.4R2.
-Prashanth