Hi,
I'm using the tool HCITester with the cc2564 and tried to do an inquiry command with the script provided.
The script works well but it seems that soms devices can discovered and some cannot (for example my HP and Fujitsu laptop will be discovered, but my Iphone 4s will not). I also tested with Iphone 6 but also not discovered. A Samsung Galaxy tablet is detected as well.
HP laptop: HCI 6.1280, LMP 6.1280 so Bluetooth version 4.0 (detected)
Fujitsu laptop: HCI 6.7869, LMP 6.64512 so Bluetooth version 4.0 (detected)
Samsung Galaxy: I can't find the HCI or LMP version, but supports Bluetooth version 3.0 (detected)
Iphone 4s or 6: I can't find the HCI or LMP version, but supports at least Bluetooth version 4.0 (not detected)
I there an Apple issue or is there a difference in Bluetooth specification?
How can I detect them as well?
Thanks in advance!
David