Other Parts Discussed in Thread: BLE-STACK
We are using CC2541 as a peripheral. Currently, we are facing very strange issue, in which our peripheral device got disconnect from iOS device immediately after connection.
The error feedback from iOS device as following:
Optional(Error Domain=CBErrorDomain Code=6 "The connection has timed out unexpectedly.
" UserInfo={NSLocalizedDescription=The connection has timed out unexpectedly.})
This device works normally in beginning, and after tested about 1 week, suddenly it reaches to the state where it disconnects immediately after connection.
But Android device still could connected to this device normally.
Our BLE-Stack version is 1.4.2
Our min. connection interval is 100ms
Our max. connection interval is 1000ms
So is there a way to fix this from peripheral side?