Using IAR EW8051 7.30b (including all patches) and it does not find a connected TI CC Debugger Target. CC Debugger (via USB) shows green light and is connected to original design cc2430 based board. Device and connected cc2430 board show up fine in TI RF Studio 7 (v1.6.1). CC Debugger firmware has been updated to version 0025. RF04EB (via USB) shows up fine in IAR when connected as debug target.
Any idea why doesn't IAR isn't finding the CC Debugger target for debug? Only thing I can think of is a CC Debugger firmware issue. Perhaps newest firmware is not recognized by older 7.30b IAR EW? Is it possible to revert to a pervious version of CC Debugger firmware? If so, any idea which one?