Hi,
Do you have a product that Sync word is corresponding to the 8bit format products Sub 1GHz band?
Best Regards,
hamada
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If you want to take advantage of the sync detect feature (Wavematch) in our CC112x/CC120x products the minimum sync word length is 11 bits. If you have an 8 bit sync word you can add the last few bits of your preamble to make up a 11 bit (or more) sync word.
Hi,Sverre.
Thank you for reply.
I would like to send a packet that is attached to the document.
In order to cope,
I want to convert to "Examination format" in the external MCU.
I believe that receiving a packet from the CC1120, and want to send the serial data to an external MCU.
The above possible?
How do I use any mode, if possible? For example, Synchronous Serial Mode?
Best Regards,
hamada
Hi,Sverre.
>The preamble + sync is 32 + 8 bits. You need to use part of the preamble as a sync word. Possible configurations:
>of preamble + sync:
How is that to insert a Preamble every time you send one frame packet?
Best Regards,
hamada
Please read the CC1120 User Guide.
You can configure CC1120 to automatically send 2 bytes of preamble + 3 bytes sync word (16 + 24 bits). On the RX side the CC1120 checks for a 3 byte sync word and starts to receive the payload as soon as the sync word is detected.