Hi,
Our customer is using CC1200 + CC1190. We got several questions from them.
1. GPIO setting and sequence to interface CC1190.
As described on AN112, customer made a connection b/w CC1200 and CC1190 as below.
- GPIO0:LNA Enable ("High" level while trasmitting)
- GPIO2:PA Enable("High" level while reciving)
- GPIO3:Mesh Interrupt
To contorl above GPIO's, what is the recommended register setting and sequence for CC1200? We are refering user guide, but above signals are not toggled.
2. Reset_N
What is minumum time for Reset signal?
3. Pull-up and Pull-down on IO
On CC1200, Is there any internal pull-up/down on IO? If yes, please let me know which PIN and resistor value?
Thanks in advance.
Regards,
Fukui