Hello everyone !
I'm using CC1110+SimpliciTI 1.2.0 on IAR and want to combine Range Extender and End Device on one device.
All this based on the Sample Application "AP as Data Hub".
I have modified the source code with:http://processors.wiki.ti.com/index.php/SimpliciTI#Compiling_with_active_END_DEVICE_and_RANGE_EXTENDER_configuration
and modify the RE source code to achieve.
And now the major problem is when I modified the config.dat of RE,
change the "-DNUM_CONNECTIONS=0 " to "-DNUM_CONNECTIONS=2" , the RE can't work.
I must change it or the device can not work as ED.
what have i got to do?
Please help me! Thanks ahead.