Hi, I just learned that FCC rules allow only a certain field strength for narrow band signals in e g the 915MHz band, corresponding to about 0 dBm ERP (i e including antenna gain) and we were hoping to use CC1101 with +10 to +12 dBm output power.
I read in datasheet §28.3 that you have tried to make the circuit compliant to this. Am I misunderstanding something? You mention only FSK here, and thus far (outside US) we have been using ASK (or on/off keying, OOK, to be precise). If I understand it correctly, we have to either have a bandwidth of >500kHz or use frequency hopping between 50 channels to be allowed to use >0dBm by FCC? With ASK I can't see how this can be done, sounds like we have to change to FSK then? Although I don't readily know what bandwidth that would give.
We need only one RF channel.