hai guys,
im using cc1200 radio module.The PER Test example has the data rates 1.2Kbps,50Kbps and 200 Kbps.I need to test for data rates upto 1Mbps.So i exported the register format in SmartRF Studio to the PER test code.i changed the LowRFsettings in PER code to 1.2Kbps from smart RF Studio(i used the 1.2mbps register settings from smart rf studio just to check whether it is working).i used Link bypass mode and could not be able to receive packets.Then,i used easy link test and i was able to receive packets.Why is that difference?