Hello,
Please let me know whether CC1310 can support 426MHz and 429MHz.
From the datasheet, 433-MHz ISM and SRD Systems can be supported.
Best Regards,
Nomoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The 433 MHz ref design is still preliminary but as the measurements show the performance looks good.
CC13xxEM-7XD-4251_0_1_0.zip433MHz Preliminary Test Report Rev 1.0.pdf
Also see https://e2e.ti.com/support/wireless_connectivity/f/156/p/472245/1697384#1697384
Hi TER,
In the reference design you've attached in your previous post, the info in the Readme file and the writing on the silk layer says it's a 425MHz design, is it ok?
I was comparing the antenna with this design (you've mentioned it in another thread) and it seems ok.
However, I want to be 100% sure this design is suitable for 433MHz.
Another thing, is there any planning on a 4 layers cc1310-433MHz design with a PCB antenna?
Thank you in advance.
hi TER
I see "CC1310 433 MHz Preliminary Performance Figures" document,it menthioned that RX sensitivity is -110.2dBm.But my testing is -108dBm, based on our own board,and the condition is simply as same as yours.
I wonder that how did you test?Our test is Using SmartRF studio 7,modify frequency from 868M to 433M, and packet RX, Observing the "Average RSSI Value". when BER > 0.1%, we consider it as a bad transmit.
Is it correct?
Thanks!