Hi,
I have read almost all the threads about OAD/OTA and CC2530 and I have some doubts about this topic.
I am working with ZStack-CC2530-2.5.0 and SmartRF05 V1.8.1 boards and using the SWRA257(V1.3) document I have run the OAD/OTA functionality to update the firmware of a ZigBee Router. (Time for .bin transmission 7-8minutes; Time for restart or update flash 2-3 minutes)
My doubts are:
- Is there any way or configuration to speed up the transmission? How?
- To update the firmware is always needed the PC (ZOAD.exe) and the Dongle or is there any other update options? -I mean, can I send the new firmware to a ZigBee Router using the PC and Dongle and after, this router be the one who resends the new firmware to other routers in the network to update the rest of the devices in the network? Any example, documentation or recommendations?
Thanks in advance for you help.