I read the Application Note AN086 and I'm so interested on using the CC2530 with CC2591.
I'm a bit confused, what is the best CC2530 Developement kit to try this solution with ZigBee?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yikai,
Thanks for your prompt response. As I read at features field:
"The CC2530 devices are preprogrammed with a Packet Error Rate (PER) test application that lets the user perform range tests with the boards. It is required to have a SmartRF05EB (from the CC2530DK) in order to run the PER test."
So, Can I reprogram the devices with a CC Debugger (or something like that) or I need a SmartRF05EB?
Best regards
For new designs we recommend CC2592 instead of CC2591. CC2592 was released earlier this year.
CC2530+CC2592 will give better sensitivity, better attenuation of harmonics, and a more robust design against load mismatch compared to a CC2530+CC2591 design.
There is a CC2538+CC2592 reference design on web. Suggest you copy the "CC2592" part of this design and combine it with the CC2530EM reference design.