The zstack define LED in hal_board_cfg as below
/* 1 - Green */
#define LED1_BV BV(0)
#define LED1_SBIT P1_0
#define LED1_DDR P1DIR
#define LED1_POLARITY ACTIVE_LOW
#if defined (HAL_BOARD_CC2530EB_REV17)
/* 2 - Red */
#define LED2_BV BV(1)
#define LED2_SBIT P1_1
#define LED2_DDR P1DIR
#define LED2_POLARITY ACTIVE_LOW
/* 3 - Yellow */
#define LED3_BV BV(4)
#define LED3_SBIT P1_4
#define LED3_DDR P1DIR
#define LED3_POLARITY ACTIVE_LOW
#endif
but actually there only one LED is work if we have use HAL_PA_PLA。
so i want to define a new LED in P15,
could you please show me the way how to config a new LED?
and please don't change the define as P11 To P15 ,just use LED2 same again。。。it was not work ,because that HAL_BOARD_CC2530EB_REV17 is collide with HAL_PA_PLA