Hi,
I'm bumping into a problem I've seen other users at "same" situation, although with different hardware or OS.
[ 38.632965] beaglebone_wl12xx_set_power() [ 39.033355] wl1271: WARNING unsupported chip id: 0x0 [ 39.043121] beaglebone_wl12xx_set_power() [ 39.082855] beaglebone_wl12xx_set_power() [ 39.483367] wl1271: WARNING unsupported chip id: 0x0 [ 39.493896] beaglebone_wl12xx_set_power() [ 39.522857] beaglebone_wl12xx_set_power() [ 39.933349] wl1271: WARNING unsupported chip id: 0x0 [ 39.942993] beaglebone_wl12xx_set_power() [ 39.952636] wl1271: ERROR firmware boot failed despite 3 retries
Please see attached my complete log:
U-Boot SPL 2013.07-dirty (Mar 10 2014 - 12:22:08) musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 OMAP SD/MMC: 0 reading args spl: error reading image args, err - -1 reading u-boot.img reading u-boot.img U-Boot 2013.07-dirty (Mar 10 2014 - 12:22:08) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled NAND: 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - readenv() failed, using default environment musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 Net: <ethaddr> not set. Validating first E-fuse MAC cpsw, usb_ether Hit any key to stop autoboot: 0 gpio: pin 53 (gpio 53) value is 1 mmc0 is current device gpio: pin 54 (gpio 54) value is 1 SD/MMC found on device 0 reading uEnv.txt 339 bytes read in 4 ms (82 KiB/s) Importing environment from mmc ... gpio: pin 55 (gpio 55) value is 1 Checking if uenvcmd is set ... gpio: pin 56 (gpio 56) value is 1 Running uenvcmd ... reading zImage 2710456 bytes read in 316 ms (8.2 MiB/s) Booting from mmc ... Kernel image @ 0x80200000 [ 0x000000 - 0x295bb8 ] Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Initializing cgroup subsys cpuset [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Linux version 3.2.42-psp27 (root@ubuntu) (gcc version 4.7.3 20130328 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.04-20130415 - Linaro GCC 2013.04) ) #4 Thu Sep 25 15:36:10 BRT 2014 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait fixrtc [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] allocated 1048576 bytes of page_cgroup [ 0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 251112k/251112k available, 11032k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc06c0000 (6880 kB) [ 0.000000] .init : 0xc06c0000 - 0xc06ff000 ( 252 kB) [ 0.000000] .data : 0xc0700000 - 0xc0747ca0 ( 288 kB) [ 0.000000] .bss : 0xc0747cc4 - 0xc078951c ( 263 kB) [ 0.000000] NR_IRQS:410 nr_irqs:410 410 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000183] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320) [ 0.048339] pid_max: default: 32768 minimum: 301 [ 0.048492] Security Framework initialized [ 0.048583] AppArmor: AppArmor initialized [ 0.048645] Mount-cache hash table entries: 512 [ 0.049102] Initializing cgroup subsys cpuacct [ 0.049163] Initializing cgroup subsys memory [ 0.049194] Initializing cgroup subsys devices [ 0.049224] Initializing cgroup subsys freezer [ 0.049224] Initializing cgroup subsys blkio [ 0.049255] Initializing cgroup subsys perf_event [ 0.049346] CPU: Testing write buffer coherency: ok [ 0.050537] devtmpfs: initialized [ 0.071197] omap_hwmod: gfx: failed to hardreset [ 0.087921] omap_hwmod: pruss: failed to hardreset [ 0.088836] print_constraints: dummy: [ 0.089141] NET: Registered protocol family 16 [ 0.090454] OMAP GPIO hardware version 0.1 [ 0.091735] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.093292] omap_i2c.1: alias fck already exists [ 0.093719] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.093933] omap2_mcspi.1: alias fck already exists [ 0.094085] omap2_mcspi.2: alias fck already exists [ 0.094177] omap_init_sham: platform not supported [ 0.094207] omap_init_aes: platform not supported [ 0.094299] edma.0: alias fck already exists [ 0.094329] edma.0: alias fck already exists [ 0.094329] edma.0: alias fck already exists [ 0.094451] cape: pcm register [ 0.104370] bio: create slab <bio-0> at 0 [ 0.105987] SCSI subsystem initialized [ 0.106994] usbcore: registered new interface driver usbfs [ 0.107147] usbcore: registered new interface driver hub [ 0.107360] usbcore: registered new device driver usb [ 0.107696] registerd cppi-dma Intr @ IRQ 17 [ 0.107727] Cppi41 Init Done Qmgr-base(d083a000) dma-base(d0838000) [ 0.107727] Cppi41 Init Done [ 0.107757] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.107940] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.108581] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.109436] tps65910 1-002d: could not be detected [ 0.110046] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.110717] NetLabel: Initializing [ 0.110717] NetLabel: domain hash size = 128 [ 0.110748] NetLabel: protocols = UNLABELED CIPSOv4 [ 0.110809] NetLabel: unlabeled traffic allowed by default [ 0.110870] Switching to clocksource gp timer [ 0.111114] AppArmor: AppArmor Filesystem Enabled [ 0.123748] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.123962] musb-hdrc musb-hdrc.0: dma type: dma-cppi41 [ 0.124176] MUSB0 controller's USBSS revision = 4ea20800 [ 0.125000] musb-hdrc musb-hdrc.0: USB OTG mode controller at d081c000 using DMA, IRQ 18 [ 0.125335] musb-hdrc musb-hdrc.1: dma type: dma-cppi41 [ 0.125518] MUSB1 controller's USBSS revision = 4ea20800 [ 0.126007] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.126129] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.126281] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.126312] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.126312] usb usb1: Product: MUSB HDRC host driver [ 0.126342] usb usb1: Manufacturer: Linux 3.2.42-psp27 musb-hcd [ 0.126342] usb usb1: SerialNumber: musb-hdrc.1 [ 0.127136] hub 1-0:1.0: USB hub found [ 0.127166] hub 1-0:1.0: 1 port detected [ 0.127685] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using DMA, IRQ 19 [ 0.128204] NET: Registered protocol family 2 [ 0.128570] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.129669] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.129882] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.130004] TCP: Hash tables configured (established 8192 bind 8192) [ 0.130004] TCP reno registered [ 0.130035] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.130065] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.130432] NET: Registered protocol family 1 [ 0.131011] RPC: Registered named UNIX socket transport module. [ 0.131042] RPC: Registered udp transport module. [ 0.131072] RPC: Registered tcp transport module. [ 0.131072] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.133300] audit: initializing netlink socket (disabled) [ 0.133361] type=2000 audit(0.130:1): initialized [ 0.336303] VFS: Disk quotas dquot_6.5.2 [ 0.336456] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.338348] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.338439] fuse init (API version 7.17) [ 0.339172] Btrfs loaded [ 0.339202] msgmni has been set to 490 [ 0.340606] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252) [ 0.340728] io scheduler noop registered [ 0.340759] io scheduler deadline registered [ 0.340850] io scheduler cfq registered (default) [ 0.342254] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.343627] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 1.047485] console [ttyO0] enabled [ 1.051849] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 1.059692] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 1.067535] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 1.075378] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 1.083221] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 1.099426] brd: module loaded [ 1.107238] loop: module loaded [ 1.110656] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.171478] No daughter card found [ 1.175109] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.190399] Board config.name: A335BONE00A60413BB000437 [ 1.195892] Board name: A335BONE [ 1.199279] Board version: 00A6 [ 1.202606] The board is a AM335x Beaglebone. [ 1.207855] tps65217 1-0024: TPS65217 ID 0xf version 1.2 [ 1.215362] print_constraints: DCDC1: 900 <--> 1800 mV at 1800 mV [ 1.223815] print_constraints: DCDC2: 900 <--> 3300 mV at 1100 mV [ 1.232208] print_constraints: DCDC3: 900 <--> 1500 mV at 1100 mV [ 1.240600] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV [ 1.248992] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV [ 1.257324] print_constraints: LDO3: 1800 <--> 3300 mV at 3300 mV [ 1.265747] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV [ 1.273101] _omap_mux_get_by_name: Could not find signal gpmc_ad8.lcd_data16 [ 1.280517] _omap_mux_get_by_name: Could not find signal gpmc_ad9.lcd_data17 [ 1.287994] _omap_mux_get_by_name: Could not find signal gpmc_ad10.lcd_data18 [ 1.295501] _omap_mux_get_by_name: Could not find signal gpmc_ad11.lcd_data19 [ 1.303039] _omap_mux_get_by_name: Could not find signal gpmc_ad12.lcd_data20 [ 1.310577] _omap_mux_get_by_name: Could not find signal gpmc_ad13.lcd_data21 [ 1.318115] _omap_mux_get_by_name: Could not find signal gpmc_ad14.lcd_data22 [ 1.325622] _omap_mux_get_by_name: Could not find signal gpmc_ad15.lcd_data23 [ 1.333404] da8xx_lcdc.0: alias fck already exists [ 1.338806] da8xx_lcdc da8xx_lcdc.0: GLCD: No valid panel found [ 1.345306] _omap_mux_get_by_name: Could not find signal NULL [ 1.351837] omap_hsmmc.0: alias fck already exists [ 1.357238] omap_i2c.2: alias fck already exists [ 1.362457] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 1.368591] omap_i2c.3: alias fck already exists [ 1.391510] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz [ 1.398132] davinci-mcasp.0: alias fck already exists [ 1.403717] Testing custom init function. (empty code) [ 1.412384] HACK!!! WIFI FORCED SETUP [ 1.416259] mmc1_wl12xx_init() [ 1.419708] TiWi WiFi cape: beaglebone_wl12xx = 1 [ 1.424682] BeagleBone cape: initializing mmc [ 1.429229] omap_hsmmc.0: alias fck already exists [ 1.434600] ------------[ cut here ]------------ [ 1.439483] WARNING: at fs/sysfs/dir.c:481 sysfs_add_one+0x80/0xa0() [ 1.446166] sysfs: cannot create duplicate filename '/devices/platform/omap/omap_hsmmc.0' [ 1.454772] Modules linked in: [ 1.458007] Backtrace: [ 1.460601] [<c0010c24>] (dump_backtrace+0x0/0x10c) from [<c04f47bc>] (dump_stack+0x18/0x1c) [ 1.469482] r6:c0114d10 r5:00000009 r4:cf037ba0 r3:60000013 [ 1.475494] [<c04f47a4>] (dump_stack+0x0/0x1c) from [<c0038b0c>] (warn_slowpath_common+0x54/0x6c) [ 1.484863] [<c0038ab8>] (warn_slowpath_common+0x0/0x6c) from [<c0038bc8>] (warn_slowpath_fmt+0x38/0x40) [ 1.494842] r8:00000000 r7:cf037be0 r6:cf251c20 r5:ffffffef r4:cf1da000 [ 1.501739] r3:00000009 [ 1.504516] [<c0038b90>] (warn_slowpath_fmt+0x0/0x40) from [<c0114d10>] (sysfs_add_one+0x80/0xa0) [ 1.513854] r3:cf1da000 r2:c063ae86 [ 1.517639] [<c0114c90>] (sysfs_add_one+0x0/0xa0) from [<c0114d94>] (create_dir+0x64/0xb8) [ 1.526336] r7:00000001 r6:cf252e10 r5:cf020b30 r4:cf251c20 [ 1.532348] [<c0114d30>] (create_dir+0x0/0xb8) from [<c0114ecc>] (sysfs_create_dir+0xb8/0xd0) [ 1.541290] r8:cf250cc0 r7:cf1c8380 r6:00000000 r5:cf020b30 r4:cf252e10 [ 1.548400] [<c0114e14>] (sysfs_create_dir+0x0/0xd0) from [<c02a4514>] (kobject_add_internal+0xbc/0x19c) [ 1.558410] r6:c0721048 r5:00000000 r4:cf252e10 [ 1.563293] [<c02a4458>] (kobject_add_internal+0x0/0x19c) from [<c02a488c>] (kobject_add+0x74/0x94) [ 1.572814] r8:cf250cc0 r7:cf1c8380 r6:c0721048 r5:00000000 r4:cf252e10 [ 1.579711] r3:00000001 [ 1.582489] [<c02a4818>] (kobject_add+0x0/0x94) from [<c03060e0>] (device_add+0xac/0x55c) [ 1.591094] r3:cf250c00 r2:00000000 [ 1.594879] r6:cf252e10 r5:00000000 r4:cf252e08 [ 1.599761] [<c0306034>] (device_add+0x0/0x55c) from [<c0309c24>] (platform_device_add+0xfc/0x164) [ 1.609222] [<c0309b28>] (platform_device_add+0x0/0x164) from [<c002aaf0>] (omap_device_register+0x24/0x2c) [ 1.619476] r7:cf1c8380 r6:c062d4d0 r5:00000000 r4:cf252e00 [ 1.625488] [<c002aacc>] (omap_device_register+0x0/0x2c) from [<c002abe8>] (omap_device_build_ss+0xf0/0x14c) [ 1.635833] [<c002aaf8>] (omap_device_build_ss+0x0/0x14c) from [<c002ac94>] (omap_device_build+0x50/0x5c) [ 1.645935] [<c002ac44>] (omap_device_build+0x0/0x5c) from [<c06cd55c>] (omap_init_hsmmc+0x594/0x6a8) [ 1.655639] [<c06ccfc8>] (omap_init_hsmmc+0x0/0x6a8) from [<c06cd6a4>] (omap2_hsmmc_init+0x34/0x48) [ 1.665191] r8:c071e5a8 r7:ffffffea r6:00000001 r5:c06f7a74 r4:c06f7aa4 [ 1.672302] [<c06cd670>] (omap2_hsmmc_init+0x0/0x48) from [<c0027684>] (mmc0_init+0x1c/0x28) [ 1.681152] r4:c0748a6c r3:60000013 [ 1.684967] [<c0027668>] (mmc0_init+0x0/0x28) from [<c00283dc>] (am335x_evm_setup+0x2dc/0x744) [ 1.694061] [<c0028100>] (am335x_evm_setup+0x0/0x744) from [<c031524c>] (at24_probe+0x3dc/0x480) [ 1.703308] r8:cf0c0a20 r7:00000000 r6:00000000 r5:cf0c0a00 r4:cf234dc0 [ 1.710388] [<c0314e70>] (at24_probe+0x0/0x480) from [<c0387380>] (i2c_device_probe+0x8c/0xb4) [ 1.719482] [<c03872f4>] (i2c_device_probe+0x0/0xb4) from [<c0308780>] (driver_probe_device+0xc0/0x19c) [ 1.729370] r5:cf0c0a54 r4:cf0c0a20 [ 1.733154] [<c03086c0>] (driver_probe_device+0x0/0x19c) from [<c03088cc>] (__driver_attach+0x70/0x94) [ 1.742980] r6:c0735fe0 r5:cf0c0a54 r4:cf0c0a20 r3:00000000 [ 1.748962] [<c030885c>] (__driver_attach+0x0/0x94) from [<c0307698>] (bus_for_each_dev+0x5c/0xa4) [ 1.758392] r6:c0735fe0 r5:cf037ee0 r4:00000000 r3:cf0146b4 [ 1.764404] [<c030763c>] (bus_for_each_dev+0x0/0xa4) from [<c0308410>] (driver_attach+0x20/0x28) [ 1.773651] r7:c073c8c8 r6:c003bd48 r5:cf234f40 r4:c0735fe0 [ 1.779632] [<c03083f0>] (driver_attach+0x0/0x28) from [<c0308034>] (bus_add_driver+0xd4/0x23c) [ 1.788787] [<c0307f60>] (bus_add_driver+0x0/0x23c) from [<c0308bb8>] (driver_register+0xa8/0x12c) [ 1.798248] [<c0308b10>] (driver_register+0x0/0x12c) from [<c0388f48>] (i2c_register_driver+0x94/0xb8) [ 1.808074] [<c0388eb4>] (i2c_register_driver+0x0/0xb8) from [<c06e120c>] (at24_init+0x48/0x54) [ 1.817230] r5:c06fe538 r4:c06fe32c [ 1.821014] [<c06e11c4>] (at24_init+0x0/0x54) from [<c0008690>] (do_one_initcall+0x9c/0x16c) [ 1.829895] [<c00085f4>] (do_one_initcall+0x0/0x16c) from [<c06c08e8>] (kernel_init+0xc4/0x168) [ 1.839050] [<c06c0824>] (kernel_init+0x0/0x168) from [<c003bd48>] (do_exit+0x0/0x608) [ 1.847381] r5:c06c0824 r4:00000000 [ 1.851196] ---[ end trace d6d716e8d4b59ffd ]--- [ 1.856079] kobject_add_internal failed for omap_hsmmc.0 with -EEXIST, don't try to register things with the same name in the same directory. [ 1.869415] Backtrace: [ 1.872009] [<c0010c24>] (dump_backtrace+0x0/0x10c) from [<c04f47bc>] (dump_stack+0x18/0x1c) [ 1.880859] r6:c0721048 r5:ffffffef r4:cf252e10 r3:60000013 [ 1.886840] [<c04f47a4>] (dump_stack+0x0/0x1c) from [<c02a4590>] (kobject_add_internal+0x138/0x19c) [ 1.896362] [<c02a4458>] (kobject_add_internal+0x0/0x19c) from [<c02a488c>] (kobject_add+0x74/0x94) [ 1.905883] r8:cf250cc0 r7:cf1c8380 r6:c0721048 r5:00000000 r4:cf252e10 [ 1.912780] r3:00000001 [ 1.915527] [<c02a4818>] (kobject_add+0x0/0x94) from [<c03060e0>] (device_add+0xac/0x55c) [ 1.924133] r3:cf250c00 r2:00000000 [ 1.927886] r6:cf252e10 r5:00000000 r4:cf252e08 [ 1.932800] [<c0306034>] (device_add+0x0/0x55c) from [<c0309c24>] (platform_device_add+0xfc/0x164) [ 1.942230] [<c0309b28>] (platform_device_add+0x0/0x164) from [<c002aaf0>] (omap_device_register+0x24/0x2c) [ 1.952453] r7:cf1c8380 r6:c062d4d0 r5:00000000 r4:cf252e00 [ 1.958435] [<c002aacc>] (omap_device_register+0x0/0x2c) from [<c002abe8>] (omap_device_build_ss+0xf0/0x14c) [ 1.968750] [<c002aaf8>] (omap_device_build_ss+0x0/0x14c) from [<c002ac94>] (omap_device_build+0x50/0x5c) [ 1.978820] [<c002ac44>] (omap_device_build+0x0/0x5c) from [<c06cd55c>] (omap_init_hsmmc+0x594/0x6a8) [ 1.988525] [<c06ccfc8>] (omap_init_hsmmc+0x0/0x6a8) from [<c06cd6a4>] (omap2_hsmmc_init+0x34/0x48) [ 1.998046] r8:c071e5a8 r7:ffffffea r6:00000001 r5:c06f7a74 r4:c06f7aa4 [ 2.005126] [<c06cd670>] (omap2_hsmmc_init+0x0/0x48) from [<c0027684>] (mmc0_init+0x1c/0x28) [ 2.014007] r4:c0748a6c r3:60000013 [ 2.017791] [<c0027668>] (mmc0_init+0x0/0x28) from [<c00283dc>] (am335x_evm_setup+0x2dc/0x744) [ 2.026855] [<c0028100>] (am335x_evm_setup+0x0/0x744) from [<c031524c>] (at24_probe+0x3dc/0x480) [ 2.036071] r8:cf0c0a20 r7:00000000 r6:00000000 r5:cf0c0a00 r4:cf234dc0 [ 2.043182] [<c0314e70>] (at24_probe+0x0/0x480) from [<c0387380>] (i2c_device_probe+0x8c/0xb4) [ 2.052246] [<c03872f4>] (i2c_device_probe+0x0/0xb4) from [<c0308780>] (driver_probe_device+0xc0/0x19c) [ 2.062133] r5:cf0c0a54 r4:cf0c0a20 [ 2.065917] [<c03086c0>] (driver_probe_device+0x0/0x19c) from [<c03088cc>] (__driver_attach+0x70/0x94) [ 2.075683] r6:c0735fe0 r5:cf0c0a54 r4:cf0c0a20 r3:00000000 [ 2.081665] [<c030885c>] (__driver_attach+0x0/0x94) from [<c0307698>] (bus_for_each_dev+0x5c/0xa4) [ 2.091064] r6:c0735fe0 r5:cf037ee0 r4:00000000 r3:cf0146b4 [ 2.097076] [<c030763c>] (bus_for_each_dev+0x0/0xa4) from [<c0308410>] (driver_attach+0x20/0x28) [ 2.106292] r7:c073c8c8 r6:c003bd48 r5:cf234f40 r4:c0735fe0 [ 2.112274] [<c03083f0>] (driver_attach+0x0/0x28) from [<c0308034>] (bus_add_driver+0xd4/0x23c) [ 2.121429] [<c0307f60>] (bus_add_driver+0x0/0x23c) from [<c0308bb8>] (driver_register+0xa8/0x12c) [ 2.130859] [<c0308b10>] (driver_register+0x0/0x12c) from [<c0388f48>] (i2c_register_driver+0x94/0xb8) [ 2.140655] [<c0388eb4>] (i2c_register_driver+0x0/0xb8) from [<c06e120c>] (at24_init+0x48/0x54) [ 2.149780] r5:c06fe538 r4:c06fe32c [ 2.153594] [<c06e11c4>] (at24_init+0x0/0x54) from [<c0008690>] (do_one_initcall+0x9c/0x16c) [ 2.162475] [<c00085f4>] (do_one_initcall+0x0/0x16c) from [<c06c08e8>] (kernel_init+0xc4/0x168) [ 2.171630] [<c06c0824>] (kernel_init+0x0/0x168) from [<c003bd48>] (do_exit+0x0/0x608) [ 2.179931] r5:c06c0824 r4:00000000 [ 2.183715] omap_device: omap_hsmmc: build failed (-17) [ 2.189208] ------------[ cut here ]------------ [ 2.194061] WARNING: at arch/arm/mach-omap2/hsmmc.c:485 omap_init_hsmmc+0x5c0/0x6a8() [ 2.202301] Can't build omap_device for omap_hsmmc:mmc1. [ 2.207855] Modules linked in: [ 2.211059] Backtrace: [ 2.213653] [<c0010c24>] (dump_backtrace+0x0/0x10c) from [<c04f47bc>] (dump_stack+0x18/0x1c) [ 2.222534] r6:c06cd588 r5:00000009 r4:cf037d58 r3:60000013 [ 2.228515] [<c04f47a4>] (dump_stack+0x0/0x1c) from [<c0038b0c>] (warn_slowpath_common+0x54/0x6c) [ 2.237854] [<c0038ab8>] (warn_slowpath_common+0x0/0x6c) from [<c0038bc8>] (warn_slowpath_fmt+0x38/0x40) [ 2.247802] r8:00003517 r7:00000001 r6:c071bc80 r5:c06f7a74 r4:cf1c8380 [ 2.254699] r3:00000009 [ 2.257476] [<c0038b90>] (warn_slowpath_fmt+0x0/0x40) from [<c06cd588>] (omap_init_hsmmc+0x5c0/0x6a8) [ 2.267150] r3:c062d4d0 r2:c0625a7f [ 2.270935] [<c06ccfc8>] (omap_init_hsmmc+0x0/0x6a8) from [<c06cd6a4>] (omap2_hsmmc_init+0x34/0x48) [ 2.280426] r8:c071e5a8 r7:ffffffea r6:00000001 r5:c06f7a74 r4:c06f7aa4 [ 2.287536] [<c06cd670>] (omap2_hsmmc_init+0x0/0x48) from [<c0027684>] (mmc0_init+0x1c/0x28) [ 2.296386] r4:c0748a6c r3:60000013 [ 2.300170] [<c0027668>] (mmc0_init+0x0/0x28) from [<c00283dc>] (am335x_evm_setup+0x2dc/0x744) [ 2.309234] [<c0028100>] (am335x_evm_setup+0x0/0x744) from [<c031524c>] (at24_probe+0x3dc/0x480) [ 2.318481] r8:cf0c0a20 r7:00000000 r6:00000000 r5:cf0c0a00 r4:cf234dc0 [ 2.325561] [<c0314e70>] (at24_probe+0x0/0x480) from [<c0387380>] (i2c_device_probe+0x8c/0xb4) [ 2.334625] [<c03872f4>] (i2c_device_probe+0x0/0xb4) from [<c0308780>] (driver_probe_device+0xc0/0x19c) [ 2.344482] r5:cf0c0a54 r4:cf0c0a20 [ 2.348266] [<c03086c0>] (driver_probe_device+0x0/0x19c) from [<c03088cc>] (__driver_attach+0x70/0x94) [ 2.358032] r6:c0735fe0 r5:cf0c0a54 r4:cf0c0a20 r3:00000000 [ 2.364044] [<c030885c>] (__driver_attach+0x0/0x94) from [<c0307698>] (bus_for_each_dev+0x5c/0xa4) [ 2.373443] r6:c0735fe0 r5:cf037ee0 r4:00000000 r3:cf0146b4 [ 2.379425] [<c030763c>] (bus_for_each_dev+0x0/0xa4) from [<c0308410>] (driver_attach+0x20/0x28) [ 2.388641] r7:c073c8c8 r6:c003bd48 r5:cf234f40 r4:c0735fe0 [ 2.394653] [<c03083f0>] (driver_attach+0x0/0x28) from [<c0308034>] (bus_add_driver+0xd4/0x23c) [ 2.403778] [<c0307f60>] (bus_add_driver+0x0/0x23c) from [<c0308bb8>] (driver_register+0xa8/0x12c) [ 2.413208] [<c0308b10>] (driver_register+0x0/0x12c) from [<c0388f48>] (i2c_register_driver+0x94/0xb8) [ 2.423004] [<c0388eb4>] (i2c_register_driver+0x0/0xb8) from [<c06e120c>] (at24_init+0x48/0x54) [ 2.432159] r5:c06fe538 r4:c06fe32c [ 2.435913] [<c06e11c4>] (at24_init+0x0/0x54) from [<c0008690>] (do_one_initcall+0x9c/0x16c) [ 2.444793] [<c00085f4>] (do_one_initcall+0x0/0x16c) from [<c06c08e8>] (kernel_init+0xc4/0x168) [ 2.453979] [<c06c0824>] (kernel_init+0x0/0x168) from [<c003bd48>] (do_exit+0x0/0x608) [ 2.462280] r5:c06c0824 r4:00000000 [ 2.466033] ---[ end trace d6d716e8d4b59ffe ]--- [ 2.470947] omap_hsmmc.1: alias fck already exists [ 2.476257] BeagleBone cape: exporting ADC pins to sysfs [ 2.482177] Beaglebone: initializing onboard LEDs [ 2.487152] BeagleBone cape: exporting SPI pins as spidev [ 2.493438] BeagleBone cape: initializing w1-gpio [ 2.498535] w1-gpio connected to P8_6 [ 2.502441] beaglebone_wl12xx_init() [ 2.506378] Configure Bluetooth Enable pin... [ 2.511322] at24 3-0054: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 2.518737] at24 3-0055: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 2.526153] at24 3-0056: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 2.533508] at24 3-0057: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 2.541931] CAN device driver interface [ 2.545959] CAN bus driver for Bosch D_CAN controller 1.0 [ 2.601562] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 2.608062] davinci_mdio davinci_mdio.0: detected phy mask fffffffe [ 2.615753] davinci_mdio.0: probed [ 2.619354] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720 [ 2.628173] usbcore: registered new interface driver cdc_ether [ 2.634399] usbcore: registered new interface driver rndis_host [ 2.640686] cdc_ncm: 04-Aug-2011 [ 2.644165] usbcore: registered new interface driver cdc_ncm [ 2.650207] Initializing USB Mass Storage driver... [ 2.655487] usbcore: registered new interface driver usb-storage [ 2.661834] USB Mass Storage support registered. [ 2.666809] usbcore: registered new interface driver libusual [ 2.672973] gadget: using random self ethernet address [ 2.678466] gadget: using random host ethernet address [ 2.685058] usb0: MAC 2e:89:4a:81:02:e0 [ 2.689086] usb0: HOST MAC 12:95:43:d3:fc:25 [ 2.693695] gadget: Ethernet Gadget, version: Memorial Day 2008 [ 2.700012] gadget: g_ether ready [ 2.703613] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 2.709289] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 2.717224] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 2.724365] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.731964] usb usb2: Product: MUSB HDRC host driver [ 2.737182] usb usb2: Manufacturer: Linux 3.2.42-psp27 musb-hcd [ 2.743408] usb usb2: SerialNumber: musb-hdrc.0 [ 2.748962] hub 2-0:1.0: USB hub found [ 2.752990] hub 2-0:1.0: 1 port detected [ 2.758056] mousedev: PS/2 mouse device common for all mice [ 2.765075] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 2.771850] omap_rtc: already running [ 2.775756] i2c /dev entries driver [ 2.780090] Linux media interface: v0.10 [ 2.784423] lirc_dev: IR Remote Control driver registered, major 249 [ 2.791198] Linux video capture interface: v2.00 [ 2.796417] Driver for 1-wire Dallas network protocol. [ 2.803924] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 2.815429] cpuidle: using governor ladder [ 2.819854] cpuidle: using governor menu [ 2.828063] usbcore: registered new interface driver usbhid [ 2.833923] usbhid: USB HID core driver [ 2.838806] usbcore: registered new interface driver snd-usb-6fire [ 2.845855] ALSA device list: [ 2.848968] No soundcards found. [ 2.853729] TCP cubic registered [ 2.857269] NET: Registered protocol family 10 [ 2.865020] NET: Registered protocol family 17 [ 2.869842] can: controller area network core (rev 20090105 abi 8) [ 2.876495] NET: Registered protocol family 29 [ 2.881134] can: raw protocol (rev 20090105) [ 2.885650] Registering the dns_resolver key type [ 2.890625] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 2.898651] ThumbEE CPU extension supported. [ 2.903167] mux: Failed to setup hwmod io irq -22 [ 2.908752] Power Management for AM33XX family [ 2.917938] registered taskstats version 1 [ 2.922637] Detected MACID=c8:a0:30:a0:61:85 [ 2.929779] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:12:10 UTC (946685530) [ 2.939300] Waiting for root device /dev/mmcblk0p2... [ 2.982482] mmc0: host does not support reading read-only switch. assuming write-enable. [ 2.992980] mmc0: new high speed SDHC card at address 1234 [ 2.999267] mmcblk0: mmc0:1234 SA04G 3.63 GiB [ 3.006286] mmcblk0: p1 p2 [ 3.010101] beaglebone_wl12xx_set_power() [ 3.159576] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem [ 3.167266] EXT4-fs (mmcblk0p2): write access will be enabled during recovery [ 3.196685] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 3.217651] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 3.225341] mmc1: new SDIO card at address 0001 [ 3.230377] beaglebone_wl12xx_set_power() [ 11.472290] EXT4-fs (mmcblk0p2): recovery complete [ 12.349822] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 12.358367] VFS: Mounted root (ext4 filesystem) readonly on device 179:2. [ 12.371978] devtmpfs: mounted [ 12.375640] Freeing init memory: 252K [ 12.724639] systemd[1]: systemd 196 running in system mode. (+PAM -LIBWRAP -AUDIT -SELINUX +IMA +SYSVINIT -LIBCRYPTSETUP +GCRYPT +ACL +XZ; angstrom) Welcome to The Ångström Distribution! [ 12.838378] systemd[1]: Inserted module 'autofs4' [ 12.846099] systemd[1]: Set hostname to <beaglebone>. [ 12.856719] systemd[1]: Initializing machine ID from random generator. [ 12.863952] systemd[1]: Installed transient /etc/machine-id file. [ 13.177032] systemd[1]: Cannot add dependency job for unit display-manager.service, ignoring: Unit display-manager.service failed to load: No such file or directory. See system logs and 'systemctl status display-manager.service' for details. [ 13.200622] systemd[1]: Starting Forward Password Requests to Wall Directory Watch. [ 13.209197] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ 13.217254] systemd[1]: Expecting device dev-ttyGS0.device... Expecting device dev-ttyGS0.device... [ 13.242584] systemd[1]: Expecting device dev-ttyO0.device... Expecting device dev-ttyO0.device... [ 13.272644] systemd[1]: Starting Syslog Socket. [ OK ] Listening on Syslog Socket. [ 13.292541] systemd[1]: Listening on Syslog Socket. [ 13.297729] systemd[1]: Starting Remote File Systems. [ OK ] Reached target Remote File Systems. [ 13.322540] systemd[1]: Reached target Remote File Systems. [ 13.328460] systemd[1]: Starting /dev/initctl Compatibility Named Pipe. [ OK ] Listening on /dev/initctl Compatibility Named Pipe. [ 13.352539] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe. [ 13.359893] systemd[1]: Starting Delayed Shutdown Socket. [ OK ] Listening on Delayed Shutdown Socket. [ 13.382537] systemd[1]: Listening on Delayed Shutdown Socket. [ 13.388702] systemd[1]: Starting Dispatch Password Requests to Console Directory Watch. [ 13.397399] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ 13.406005] systemd[1]: Starting Arbitrary Executable File Formats File System Automount Point. [ OK ] Set up automount Arbitrary Executable File Formats F...utomount Point. [ 13.442626] systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point. [ 13.453155] systemd[1]: Starting udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 13.482635] systemd[1]: Listening on udev Kernel Socket. [ 13.488708] systemd[1]: Starting udev Control Socket. [ OK ] Listening on udev Control Socket. [ 13.512634] systemd[1]: Listening on udev Control Socket. [ 13.518371] systemd[1]: Starting Swap. [ OK ] Reached target Swap. [ 13.542602] systemd[1]: Reached target Swap. [ 13.547210] systemd[1]: Starting Journal Socket. [ OK ] Listening on Journal Socket. [ 13.572662] systemd[1]: Listening on Journal Socket. [ 13.577972] systemd[1]: Starting Syslog. [ OK ] Reached target Syslog. [ 13.602630] systemd[1]: Reached target Syslog. [ 13.607452] systemd[1]: Starting File System Check on Root Device... Starting File System Check on Root Device... [ 13.636169] systemd[1]: Starting udev Kernel Device Manager... Starting udev Kernel Device Manager... [ 13.666046] systemd[1]: Started Machine ID first boot configure. [ 13.672485] systemd[1]: Mounting Debug File System... Mounting Debug File System... [ 13.705871] systemd[1]: Starting udev Coldplug all Devices... Starting udev Coldplug all Devices... [ 13.737030] systemd[1]: Mounted Huge Pages File System. [ 13.746887] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 13.779876] systemd[1]: Starting Journal Service... Starting Journal Service... [ OK ] Started Journal Service. [ 13.832916] systemd[1]: Started Journal Service. [ 13.850097] systemd[1]: Starting Apply Kernel Variables... Starting Apply Kernel Variables... [ 13.891448] systemd-udevd[52]: starting version 196 [ 14.133209] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 14.169128] systemd[1]: Started Set Up Additional Binary Formats. [ OK ] Started udev Kernel Device Manager. [ 14.213043] systemd[1]: Started udev Kernel Device Manager. [ OK ] Mounted Debug File System. [ 14.243072] systemd[1]: Mounted Debug File System. [ OK ] Mounted POSIX Message Queue File System. [ 14.263671] systemd[1]: Mounted POSIX Message Queue File System. [ 14.284973] Bluetooth: Core ver 2.16 [ 14.288818] NET: Registered protocol family 31 [ 14.293518] Bluetooth: HCI device and connection manager initialized [ 14.300140] Bluetooth: HCI socket layer initialized [ 14.305267] Bluetooth: L2CAP socket layer initialized [ 14.310546] Bluetooth: SCO socket layer initialized [ OK ] Started Apply Kernel Variables. [ 14.343170] systemd[1]: Started Apply Kernel Variables. [ 14.379455] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 systemd-fsck[50]: rootfs: clean, 117898/235248 files, 629473/940800 blocks [ 14.479583] NET: Registered protocol family 23 [ OK ] Started File System Check on Root Device. Starting Remount Root and Kernel File Systems... [ 14.577972] IrCOMM protocol (Dag Brattli) [ OK ] Started udev Coldplug all Devices. [ 14.659332] Bluetooth: RFCOMM TTY layer initialized [ 14.664550] Bluetooth: RFCOMM socket layer initialized [ 14.669921] Bluetooth: RFCOMM ver 1.11 [ OK 14.680450] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) m] Started Load Kernel Modules. Mounting FUSE Control File System... [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Mounted FUSE Control File System. [ OK ] Reached target Local File Systems (Pre). Mounting /tmp... Starting Load Random Seed... [ OK ] Mounted /tmp. [ OK ] Reached target Local File Systems. Starting Recreate Volatile Files and Directories... Starting Trigger Flushing of Journal to Persistent Storage... [ OK ] Started Load Random Seed. [ 15.027709] systemd-journald[56]: Received SIGUSR1 [ OK ] Started Recreate Volatile Files and Directories. [ OK ] Started Trigger Flushing of Journal to Persistent Storage. [ OK ] Reached target System Initialization. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Restore Sound Card State... [ OK ] Listening on bonescript.socket. [ OK ] Listening on dropbear.socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. Starting Periodic Command Scheduler... [ OK ] Started Periodic Command Scheduler. Starting Connection service... Starting Start usb mass storage gadget... [ OK ] Started Start usb mass storage gadget. Starting Angstrom LED config... [ OK ] Started Angstrom LED config. Starting Cloud9 IDE... [ OK ] Started Cloud9 IDE. Starting Music Player Daemon... [ OK ] Started Music Player Daemon. Starting Network Time Service (one-shot ntpdate mode)... Starting Bonescript autorun... [ OK ] Started Bonescript autorun. Starting D-Bus System Message Bus... [ OK ] Started D-Bus System Message Bus. Starting Login Service... Starting Permit User Sessions... Starting Kernel Logging Service... [ OK ] Started Kernel Logging Service. Starting System Logging Service... [ OK ] Started System Logging Service. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started Restore Sound Card State. [ OK ] Started Network Time Service (one-shot ntpdate mode). [ OK ] Started Permit User Sessions. Starting Getty on tty1... [ OK ] Started Getty on tty1. [ OK ] Started Connection service. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started Login Service. [ 18.234924] ip_tables: (C) 2000-2006 Netfilter Core Team [ OK ] Found device /dev/ttyO0. [ 18.333160] nf_conntrack version 0.5.0 (3927 buckets, 15708 max) Starting Serial Getty on ttyO0... [ OK ] Started Serial Getty on ttyO0. [ 19.114929] systemd-udevd[52]: worker [60] terminated by signal 11 (Segmentation fault) [ 19.128692] systemd-udevd[52]: worker [60] failed while handling '/devices/platform/omap/musb-ti81xx/musb-hdrc.0/gadget/net/usb0' [ 21.069763] cfg80211: Calling CRDA to update world regulatory domain [ 21.076660] cfg80211: World regulatory domain updated: [ 21.082061] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) [ 21.090850] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 21.099151] cfg80211: (2457000 KHz - 2482000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 21.107482] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 21.115783] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 21.124114] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 22.443908] beaglebone_wl12xx_set_power() [ 29.113250] wl1271: loaded [ 29.116363] beaglebone_wl12xx_set_power() [ 29.125640] ADDRCONF(NETDEV_UP): usb0: link is not ready .---O---. | | .-. o o | | |-----.-----.-----.| | .----..-----.-----. | | | __ | ---'| '--.| .-'| | | | | | | | |--- || --'| | | ' | | | | '---'---'--'--'--. |-----''----''--' '-----'-'-'-' -' | '---' The Angstrom Distribution beaglebone ttyO0 Angstrom v2012.12 - Kernel 3.2.42-psp27 beaglebone login: Starting WPA supplicant... [ OK ] Started WPA supplicant. [ 37.129364] [ 37.129364] CPSW phy found : id is : 0x7c0f1 [ 37.136199] PHY 0:01 not found [ 37.140380] ADDRCONF(NETDEV_UP): eth0: link is not ready [ 37.282867] beaglebone_wl12xx_set_power() [ 37.683380] wl1271: WARNING unsupported chip id: 0x0 [ 37.692840] beaglebone_wl12xx_set_power() [ 37.722808] beaglebone_wl12xx_set_power() [ 38.123962] wl1271: WARNING unsupported chip id: 0x0 [ 38.136657] beaglebone_wl12xx_set_power() [ 38.172851] beaglebone_wl12xx_set_power() [ 38.573394] wl1271: WARNING unsupported chip id: 0x0 [ 38.582794] beaglebone_wl12xx_set_power() [ 38.592315] wl1271: ERROR firmware boot failed despite 3 retries [ 38.632965] beaglebone_wl12xx_set_power() [ 39.033355] wl1271: WARNING unsupported chip id: 0x0 [ 39.043121] beaglebone_wl12xx_set_power() [ 39.082855] beaglebone_wl12xx_set_power() [ 39.483367] wl1271: WARNING unsupported chip id: 0x0 [ 39.493896] beaglebone_wl12xx_set_power() [ 39.522857] beaglebone_wl12xx_set_power() [ 39.933349] wl1271: WARNING unsupported chip id: 0x0 [ 39.942993] beaglebone_wl12xx_set_power() [ 39.952636] wl1271: ERROR firmware boot failed despite 3 retries [ TIME ] Timed out waiting for device dev-ttyGS0.device. [DEPEND] Dependency failed for Serial Getty on ttyGS0. [ OK ] Reached target Login Prompts. [ OK ] Reached target Multi-User. [ OK ] Reached target Graphical Interface.
I know I need to ensure the correct firmware is at the right place, but I didn't find the information about which firmware is the right one for me (nor any information about firmware). Also, I've seen the clock frequency could be changed in order to overcome integrity signal issues, but I couldn't find information about where is the right piece of code to do this modification.
I'm working with Linux, AM3359 and the TIWI-BLE module.
Thanks!
Best Regards,
Victor Leite