Hi,
I am working on making a wireless speaker system using the CC8530. I know that the CC8530 can support 4 channels and therefore 4 slaves. If I am streaming to the master via another wireless technology, I should be able to really have 5 speakers in a system correct? The real question is can the Master CC8530 board output to a speaker directly?
Also, if I want to be able to set up each speaker as the master or slave, would I need to have a master and a slave in each speaker since I know they cannot switch roles. However, can a slave be configured to connect to multiple masters (not at the same time, but go from streaming from one master to another)? The configuration I want is so any speaker in the system can serve as the master or as a slave.
Thanks,
David