Hello
I'm trying out OAD on the cc2541.
Using the project of BLE-CC254x-1.3.2 SensorTag
Refferred to OAD_for_CC254x.pdf , following the steps. There are two fault shows :
1. When I set the link -> Extra output , check the box override default, I try to buid ,but it says this
"Fatal Error[e62]: File name "C:\Texas Instruments\BLE-CC254x- 1.3.2\Projects\ble\SensorTag\CC2541DB\
CC2541DK-Sensor-OAD-ImgA\Exe\SensorTag.hex used for multiple files "
The hex file is used for multiple files. If I uncheck the override default, it can work well ,but I meet the second problem.
2. when I try to make ,it always show "Performing Post-Build Action "
pls help me!
Thanks!